Other Parts Discussed in Thread: AM3357, AM3352
最近设计了一块AM5716的CPU板,是从AM571X IDK优化的。无法从SD卡启动。
SYSBOOT【5:0】=0b100010, 串口上没有反应。
后来改成从串口启动
SYSBOOT【5:0】=0b010011, 串口上接收到JE!, 串口设置115200,8,E,1,no flow control.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SYSBOOT配置没有问题。
从uart启动有JE!打印是正常的,说明ROM正在尝试启动。关于uart启动部分可参考附件的ppt看一下。
5342.AM57_UART_Boot_SOP_By_TI_Rio_Final.pdf
另外尝试SD卡启动时可以先用SDK中预编译好的镜像文件尝试。
1、我以前用AM3352跟AM3357上电都是默认打印CCC的。AM5716我看论坛上很多上电也是打印CCC。不知道我板子打印JE!是什么差异造成的?
2、我们SD卡用在Demo上是可以启动的;
3、PPT中serial-boot.pl跟u-boot-spl.bin在哪里可以下载?
我以前用AM3352跟AM3357上电都是默认打印CCC的。AM5716我看论坛上很多上电也是打印CCC。不知道我板子打印JE!是什么差异造成的?
是正常的,有过相关确认。
I checked with the RoM expert and JE! is on UART console means its behaving as expected
in the UART boot mode. So no issues with the MPU there.
、我们SD卡用在Demo上是可以启动的;
是自制的镜像文件不可以启动吗?
PPT中serial-boot.pl跟u-boot-spl.bin在哪里可以下载?
u-boot-spl.bin 在uboot文件夹下找找。