SDK 版本:ti-processor-sdk-linux-rt-am335x-evm-07.03.00.005
硬件:beaglebone black BBVIEW+4.3寸屏幕(使用非设备树的老版本SDK测试功能完好)
运行 自带QT 程序报错(已设置相关环境变量):
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
root@am335x-evm:/usr/share/examples/gui/analogclock# sudo ./analogclock \
> -platform eglfs
QStandardPaths: XDG_RUNTIME_DIR not set, defaulting to '/tmp/runtime-root'
Failed to move cursor on screen LVDS1: -13
qt.qpa.input: xkbcommon not available, not performing key mapping
Attribute Qt::AA_ShareOpenGLContexts must be set before QCoreApplication is cre.
Could not set DRM mode for screen LVDS1 (Permission denied)
Could not queue DRM page flip on screen LVDS1 (Permission denied)
Could not queue DRM page flip on screen LVDS1 (Permission denied)
Could not queue DRM page flip on screen LVDS1 (Permission denied)
Could not queue DRM page flip on screen LVDS1 (Permission denied)
Could not queue DRM page flip on screen LVDS1 (Permission denied)
^X^XCould not queue DRM page flip on screen LVDS1 (Permission denied)
那边论坛没有回复,你们帮看一下吧。
我尝试把weston关掉 ,使用 linuxfb 运行程序:
root@am335x-evm:/usr/share/examples/gui/analogclock# sudo ./analogclock -platform linuxfb
显示正常。
但是现在ti的sdk里面已经支持sgx的drm驱动,eglfs下的错误如何解决?
Could not queue DRM page flip on screen LVDS1 (Permission denied)
你好,感谢的帮助,那边工程师给了回复,按照他的方法可以正常显示qt example了,但是有个问题:
关闭了weston以后,触摸屏一直不对,我移植了tslib,并完成了5点校准,但是启动qt程序后坐标还是偏移比较大。
我看了一下以前的帖子,原因是SDK中触摸屏是基于weston的:e2echina.ti.com/.../yocto-project-qt5-tslib
是不是我要重新编译qt?