This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748的不同版本对应工作电压

Other Parts Discussed in Thread: TMS320C6748

TMS320C6748的版本根据速度等级有375MHz和456MHz两种,在datasheet第76页看到Internal RAM Supply Voltage 对于375MHz和456MHz版本不一样。

我想请问:

1、456MHz Version的器件,RVDD必须选用1.3V吗,即使器件主频工作在375MHz?

2、375MHz Version的器件,如果CVDD使用1.3V,是否可以工作到456MHz,此时RVDD又该选用多少?

  • 芯片的最高主频是由芯片本身决定的,不是供电电压决定的,因此要看芯片了。比如最高主频可达456M,375M,这个是不可以改变的。

    RVDD也是和芯片匹配的,不同版本的芯片,电压要符合规定。