This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TDA4VM: 如何从 QSPI 引导?

Part Number: TDA4VM


问:默认 SDK 支持从 OSPI (OSPI0) 引导。如何从 QSPI(也称为 OSPI1)引导。需要在 u-boot 中


进行哪些更改?

  • 答:是的,支持从 QSPI 引导。默认情况下,U-Boot/SPL 配置为从 OSPI(OSPI0) 引导。因此,我们需要在 U-Boot 目录中进行以下更改:

    From fa016786d99db486f14c491927ad582eb940467b Mon Sep 17 00:00:00 2001

    From: Keerthy <j-keerthy@ti.com>

    Date: Thu, 2 Sep 2021 10:06:31 +0530

    Subject: [PATCH] configs: Enable QSPI

     

    Enable QSPI

     

    Signed-off-by: Keerthy <j-keerthy@ti.com>

    ---

     configs/j721e_evm_a72_defconfig | 1 +

     configs/j721e_evm_r5_defconfig  | 1 +

     2 files changed, 2 insertions(+)

     

    diff --git a/configs/j721e_evm_a72_defconfig b/configs/j721e_evm_a72_defconfig

    index 8f16ae354e..8c9631cd24 100644

    --- a/configs/j721e_evm_a72_defconfig

    +++ b/configs/j721e_evm_a72_defconfig

    @@ -72,6 +72,7 @@ CONFIG_CMD_UBI=y

     CONFIG_OF_CONTROL=y

     CONFIG_SPL_OF_CONTROL=y

     CONFIG_DEFAULT_DEVICE_TREE="k3-j721e-common-proc-board"

    +CONFIG_SF_DEFAULT_BUS=1

     CONFIG_OF_LIST="k3-j721e-common-proc-board k3-j721e-tps65917-proc-board"

     CONFIG_SPL_MULTI_DTB_FIT=y

     CONFIG_SPL_MULTI_DTB_FIT_NO_COMPRESSION=y

    diff --git a/configs/j721e_evm_r5_defconfig b/configs/j721e_evm_r5_defconfig

    index bb3d1a28c6..901d8b76ce 100644

    --- a/configs/j721e_evm_r5_defconfig

    +++ b/configs/j721e_evm_r5_defconfig

    @@ -60,6 +60,7 @@ CONFIG_CMD_FAT=y

     CONFIG_OF_CONTROL=y

     CONFIG_SPL_OF_CONTROL=y

     CONFIG_DEFAULT_DEVICE_TREE="k3-j721e-r5-common-proc-board"

    +CONFIG_SF_DEFAULT_BUS=1

     CONFIG_ENV_IS_IN_MMC=y

     CONFIG_SYS_RELOC_GD_ENV_ADDR=y

     CONFIG_DM=y

    --

    2.17.1

    *****************************************************************************

    cd $PSDKLA_PATH/board-support/u-boot-2020.01+gitAUTOINC+2781231a33-g2781231a33

    git am 0001-configs-Enable-QSPI.patch.txt

    cd ../..

    make u-boot

     

    cp board-support/u-boot_build/a72/tispl.bin board-support/u-boot_build/a72/u-boot.img board-support/prebuilt-binaries/sysfw.itb board-support/u-boot_build/r5/tiboot3.bin /media/$USER/boot/

     

    将新编译的二进制文件复制到 SD 卡的引导分区中后,使用 SD Boot 引导至 u-boot 提示符:


    DIP 开关设置:


    SW8:10000010


    SW9:00000000


    引导至 U-Boot 提示符:

    sf probe 1:0 /* this is for QSPI */

     

    fatload mmc 1 ${loadaddr} tiboot3.bin; sf update $loadaddr 0x0 $filesize;

    fatload mmc 1 ${loadaddr} tispl.bin; sf update $loadaddr 0x80000 $filesize;

    fatload mmc 1 ${loadaddr} u-boot.img; sf update $loadaddr 0x280000 $filesize;

    fatload mmc 1 ${loadaddr} sysfw.itb; sf update $loadaddr 0x6C0000 $filesize

     

    刷写 QSPI 后,请关闭电路板并按如下所示更改 DIP 开关设置:


    SW8:00000000


    SW9:00100000

    导通电路板。在从 SPI 引导时,您可以观察到以下情况:

    U-Boot SPL 2020.01-00002-g8903f0640e-dirty (Aug 09 2021 - 15:42:23 +0530)

    SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')

    Trying to boot from SPI

    Loading Environment from MMC...*** Warning - No MMC card found, using default environment

     

    Starting ATF on ARM64 core...

     

    NOTICE:  BL31: v2.4(release):07.03.00.005-dirty

    NOTICE:  BL31: Built : 00:15:40, Apr 10 2021

     

    U-Boot SPL 2020.01-00002-g8903f0640e-dirty (Aug 09 2021 - 15:42:15 +0530)

    SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')

    Detected: J7X-BASE-CPB rev E2

    Detected: J7X-INFOTAN-EXP rev E3

    Detected: J7X-VSC8514-ETH rev E2

    Trying to boot from SPI

    Can't get reset: -2

    Software reset enable failed: -524

     

     

    U-Boot 2020.01-00002-g8903f0640e-dirty (Aug 09 2021 - 15:42:15 +0530)

     

    SoC:   J721E SR1.0

    Model: Texas Instruments K3 J721E SoC

    Board: J721EX-PM2-SOM rev E6

    DRAM:  4 GiB

    not found for dev hbmc-mux

    Flash: 0 Bytes

    MMC:   sdhci@4f80000: 0, sdhci@4fb0000: 1

    Loading Environment from MMC...OK

    In:    serial@2800000

    Out:   serial@2800000

    Err:   serial@2800000

    Detected: J7X-BASE-CPB rev E2

    Detected: J7X-INFOTAN-EXP rev E3

    Detected: J7X-VSC8514-ETH rev E2

    Net:   K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000

     

    Warning: ethernet@46000000 using MAC address from ROM

    eth0: ethernet@46000000

    Hit any key to stop autoboot:  0