This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: C6748通过EMIF连接FPGA

Part Number: TMS320C6748

C6748通过EMIF连接FPGA,在FPGA内设计一个FIFO,目前想把EMIF设置为同步模式,在同步模式下实现FIFO数据读写操作。C6748只有CS0为同步模式,可否将CS0连接FIFO的rd_en(读使能),EMIF时钟EMA_CLK连接FIFO的rd_clk(读时钟),EMIF总线连接FIFO的dout[0:15],不知是否可以这样设计?

  • 我已转给其他工程师确认。

  • 不行。

    C6748上的EMIF CS0的同步模式仅仅是支持SDRAM时序。不像AM335x上的GPMC,那是支持同步时序的。

    如果是在FPGA端实现FIFO,在C6748端用EDMA进行连续访问,速度也是可以的。

    EMIF时钟EMA_CLK是可以连续输出的,不管是否用CS0。