This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于c6670 srio 1port 4x device和4port 1x device管脚连接问题



专家,您好。

c6670DSP上srio管脚从0~3进行了编号,即RIOTX3...RIOTX0 和RIORX3...RIORX0,当6670dsp和FPGA(Xilinx spartan45t或者spartan75t)通过srio连接时,在1port 4xdevice情况下,在硬件管脚连接上有对应关系吗?比如dsp侧的RIOTX0和RIORX0只能对应FPGA侧的TX0/RX0,这样1对1,2对2,3对3,还是说没有对应关系要求,dsp侧的RIOTX0和RIORX0可以和FPGA侧的任何一对收发管脚相接?在4port1xdevice情况下又是怎样的?我们现在在做硬件设计,涉及到管脚连接,布线方面的考虑,有这个疑问,需要确认一下,谢谢。