CPU的1.8V电源通过TPS65070的LDO1提供,系统启动后,电源芯片发热严重。在3.3v电路中串联5.2欧姆电阻测得电流是100多mA(还有为其它电路供电),1.8V电路中串联进这个电阻后,在CPU管脚一端的电压竟然达到了2.2V左右。好像是电压从CPU出来的一样,好几个板子都是这样,求解!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
再说明一下,系统是可以正常工作的,程序也跑得通。就是电源芯片发热。
这两天查了一下,只要bootloader中打开ddrII控制器的电源,TPS65070马上就开始发热。我用LM1117-1.8V代替系统1.8V电源,LM1117芯片也发热,但是TPS65070温度就正常了。是什么原因导致了1.8V电源消耗这么大?1.8V电压只给DDR-II芯片和CPU的DDR控制器供电,IO口是3.3V。我看到DDR-II是SSTL电平,mDDR是LVCMOS电平,这一点我已经在DDR_SLEW中设置好了,没有任何变化。
急!求解!
你好!请在设计前仔细阅读芯片的勘误表
http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=sprz301h&fileType=pdf
在Advisory 2.1.18中有详述,1.8v电源输出侧,靠近芯片处需要加一个大电容。