采用DM365ImageTuningTooll工具在色温箱里完成白平衡矫正,得到的矫正参数,应用到白炽灯环境中,出现色彩浓烈;把WB的offset全部设置为0,又出现画面偏朦胧的情况;请问WB的offset参数有什么作用,白平衡又该如何调节?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用DM365ImageTuningTooll工具在色温箱里完成白平衡矫正,得到的矫正参数,应用到白炽灯环境中,出现色彩浓烈;把WB的offset全部设置为0,又出现画面偏朦胧的情况;请问WB的offset参数有什么作用,白平衡又该如何调节?
这个offset是tuning出来的,你不应该手动去修改它,
上图你减了100多自然会偏暗,下面你又完全不减,
那你在调试白平衡之前黑电平校准准确了没有呢?
黑电平经过校正后,设置参数为-3,默认设置是0。
但是效果依然是一样的。
在图中的顶部是使用DM365ImageTuningTooll工具得到的参数,没有手动修改的,但是色彩鲜明并且局部偏暗;
在图中的底部,之所以把offset设置为0,那是因为TI_aewb_ISP.c中并没有对offset设置,默认设置是0;
请问在使用DM365ImageTuningTooll进行白平衡设置的时候,需要注意什么?