我用的是官方的EVM板,我的SW5的设置是off ,也就是拨码开关都设置为靠近PCIE插座。在这种设置下,当我插了PCIE网卡(x1),上电串口竟然无反应,此PCIE网卡我已经在PC机上测试过了,可以使用。以下是我不插PCIE网卡的时候串口打印信息。
Linux version 2.6.37 (root@ubuntu) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #21 Mon May 6 11:39:25 CST 2013
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 2.0
On node 0 totalpages: 80384
free_area_init_node: node 0, pgdat c0590158, node_mem_map c05cc000
Normal zone: 728 pages used for memmap
Normal zone: 0 pages reserved
Normal zone: 79656 pages, LIFO batch:15
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 79656
Kernel command line: console=ttyO2,115200n8 rootwait root=/dev/sda1 rw mem=364M@0x80000000 324M@0x9F900000 notifyk.vpssm3_sva=0xBF900000 ip=off noinitrd
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 314MB = 314MB total
Memory: 312248k/312248k available, 60488k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd7000000 - 0xf8000000 ( 528 MB)
lowmem : 0xc0000000 - 0xd6c00000 ( 364 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc003d000 ( 212 kB)
.text : 0xc003d000 - 0xc0546000 (5156 kB)
.data : 0xc0546000 - 0xc0591b40 ( 303 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
NOR: Can't request GPMC CS
registered ti816x_gpio_vr device
registered ti816x_sr device
clk get on i2c3 fck failed
_omap_mux_get_by_name: Could not find signal dcan0_tx.dcan0_tx
_omap_mux_get_by_name: Could not find signal dcan0_rx.dcan0_rx
pm_dbg_init: only OMAP3 supported
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd7020000
ti81xx_pcie: Setting outbound translation for 0x20000000-0x2fffffff
ti81xx_pcie: Starting PCI scan...
pci_bus 0000:00: scanning bus
ti81xx_pcie: Reading config[0] for device 0000:00:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:01:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:02:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:03:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:04:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:05:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:06:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:07:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:08:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:09:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:0a:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:0b:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:0c:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:0d:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:0e:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:0f:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:10:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:11:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:12:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:13:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:14:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:15:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:16:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:17:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:18:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:19:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:1a:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:1b:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:1c:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:1d:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:1e:00..
failed. No link/device.
ti81xx_pcie: Reading config[0] for device 0000:1f:00..
failed. No link/device.
pci_bus 0000:00: fixups for bus
PCI: bus0: Fast back to back transfers enabled
pci_bus 0000:00: bus scan returning with max=00
pci_bus 0000:00: resource 0 [mem 0x20000000-0x2fffffff]
pci_bus 0000:00: resource 1 [io 0x40000000-0x402fffff]
bio: create slab <bio-0> at 0
regulator: VFB: 800 <--> 1025 mV at 1010 mV
vgaarb: loaded
SCSI subsystem initialized
libata version 3.00 loaded.
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
USBSS revision 4ea20809
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
TxFifo Empty intr disabled
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d701e000 using DMA, IRQ 18
Registered /proc/driver/musb_hdrc.0
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
TxFifo Empty intr disabled
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d7026800 using DMA, IRQ 19
Registered /proc/driver/musb_hdrc.1
NET: Registered protocol family 2
IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
TCP established hash table entries: 16384 (order: 5, 131072 bytes)
TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PCI: CLS 0 bytes, default 64
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 609
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
ti81xx_pcie_ep: No TI81xx PCIe EP [0xb800] found
ti81xx_pcie_ep: No TI81xx PCIe EP [0xb801] found
ti81xx_pcie_ep: No TI81xx PCIe EP found.
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x3
ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
scsi1 : ahci_platform
ata1: SATA max UDMA/133 irq_stat 0x00400040, connection status changed irq 16
ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
m25p80 spi1.0: found w25q32, expected m25p80
m25p80 spi1.0: w25q32 (4096 Kbytes)
Creating 4 MTD partitions on "spi_flash":
0x000000000000-0x000000040000 : "U-Boot"
0x000000040000-0x000000042000 : "U-Boot Env"
0x000000042000-0x0000002c2000 : "Kernel"
0x0000002c2000-0x000000400000 : "File System"
omap2-nand driver initializing
ONFI flash detected
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff9
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver smsc95xx
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
uhci_hcd: USB Universal Host Controller Interface driver
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
usb 1-1: new full speed USB device using musb-hdrc and address 2
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbf900000
usbcore: registered new interface driver snd-usb-audio
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
smartreflex smartreflex: Driver initialized
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
ata2: SATA link down (SStatus 0 SControl 300)
mmc0: new high speed SD card at address cffe
mmcblk0: mmc0:cffe SD02G 1.83 GiB
usb 1-1: New USB device found, idVendor=05e3, idProduct=0606
usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 1-1: Product: USB Hub 2.0
usb 1-1: Manufacturer: ALCOR
mmcblk0: p1 p2 p3
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 4 ports detected
usb 1-1.2: new low speed USB device using musb-hdrc and address 3
usb 1-1.2: New USB device found, idVendor=0425, idProduct=0001
usb 1-1.2: New USB device strings: Mfr=0, Product=1, SerialNumber=0
usb 1-1.2: Product: USB OPTICAL MOUSE
input: USB OPTICAL MOUSE as /devices/platform/omap/ti81xx-usbss/musb-hdrc.0/usb1/1-1/1-1.2/1-1.2:1.0/input/input0
generic-usb 0003:0425:0001.0001: input: USB HID v1.11 Mouse [ USB OPTICAL MOUSE] on usb-musb-hdrc.0-1.2/input0
ata1: link is slow to respond, please be patient (ready=0)
ata1: softreset failed (device not ready)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1.00: ATA-8: Hitachi HTS545032B9A300, PB3OC64G, max UDMA/133
ata1.00: 625142448 sectors, multi 0: LBA48 NCQ (depth 31/32)
ata1.00: configured for UDMA/133
scsi 0:0:0:0: Direct-Access ATA Hitachi HTS54503 PB3O PQ: 0 ANSI: 5
sd 0:0:0:0: Attached scsi generic sg0 type 0
sd 0:0:0:0: [sda] 625142448 512-byte logical blocks: (320 GB/298 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Mode Sense: 00 3a 00 00
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
sda: sda1 sda2 sda3
sd 0:0:0:0: [sda] Attached SCSI disk
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (sda1): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (sda1): using internal journal
EXT3-fs (sda1): recovery complete
EXT3-fs (sda1): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 8:1.
devtmpfs: mounted
Freeing init memory: 212K
udevd (90): /proc/90/oom_adj is deprecated, please use /proc/90/oom_score_adj instead.
udev: starting version 141
minix: disagrees about version of symbol module_layout
minix: disagrees about version of symbol module_layout
FAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev mmcblk0.
EXT3-fs (mmcblk0): error: can't find ext3 filesystem on dev mmcblk0.
EXT2-fs (mmcblk0): error: can't find an ext2 filesystem on dev mmcblk0.
FAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev mmcblk0.
NET: Registered protocol family 10
ISOFS: Unable to identify CD-ROM format.
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (sda3): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs: barriers not enabled
EXT3-fs (sda3): using internal journal
EXT3-fs (sda3): recovery complete
EXT3-fs (sda3): mounted filesystem with writeback data mode
kjournald starting. Commit interval 5 seconds
EXT3-fs (sda2): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (sda2): using internal journal
EXT3-fs (sda2): recovery complete
EXT3-fs (sda2): mounted filesystem with writeback data mode
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)
ADDRCONF(NETDEV_UP): eth0: link is not ready
net eth0: DaVinci EMAC: ioctl not supported
net eth0: DaVinci EMAC: ioctl not supported
net eth1: DaVinci EMAC: ioctl not supported
SysLink version : 2.10.03.20
SysLink module created on Date:Apr 29 2012 Time:20:45:11
PHY: 0:01 - Link is Up - 100/Full
ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
HDMI W1 rev 2.0
hdmi: Enter HDMI_W1_StopVideoFrame()
found best resolution: 1680x1050 (31)
Extension block present db 2 23
84
Extension block present db 1 23
84
Extension block present db 3 23
84
Extension block present db 3 23
84
Extension block present db 3 23
84
hdmi: Enter HDMI_W1_GlobalInitVars()
hdmi: Enter HDMI_Core_GlobalInitVars()
hdmi: Enter HDMI_W1_ConfigVideoResolutionTiming()
hdmi: Enter HDMI_W1_ConfigVideoInterface()
hdmi: HDMI_WP_AUDIO_CFG = 0x1030006
hdmi: HDMI_WP_AUDIO_CFG2 = 0x20c0
hdmi: HDMI_WP_AUDIO_CTRL = 0x20
hdmi: Enter DSS_HDMI_CORE_SW_RESET_ASSERT ()
hdmi: Enter DSS_HDMI_CORE_POWER_DOWN_DISABLE()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_RELEASE()
hdmi: Enter HDMI_W1_StartVideoFrame ()
hdmi: Irqenable 60000011
hdmi: 40 hpd
hdmi: -------------DEBUG-------------------
hdmi: 1 hdmi_wp_irqstatus
hdmi: 1 hdmi_core_intr_state
hdmi: 60 hdmi_core_intr1
hdmi: 3 hdmi_core_intr2
hdmi: f hdmi_core_intr3
hdmi: 87 hdmi_core_sys_sys_stat
hdmi: -------------DEBUG-------------------
hdmi: first hpd
net eth1: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:02, id=282f014)
ADDRCONF(NETDEV_UP): eth1: link is not ready
PHY: 0:02 - Link is Up - 100/Full
ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
eth0: no IPv6 routers present
eth1: no IPv6 routers present
root@luhao:~#
求助...我的PCIE网卡是RTL8111C的。