您好,当我想通过数据空间(DATA)去访问外部存储器时,是否可以做到?因为我的外部存储器片选,读写信号连接在5416的notDS和RW信号上,我阅读其芯片手册发现,访问外部空间需要将DROM信号置为1,我依据手册这样做了,但是我不了解我访问的0x8000是否对于外部存储器来说也是0x8000?我通过示波器测量相应A15信号,发现其无信号。又尝试了0x8001,0x8003,0xFFFF,都无法在地址线上查到相关信号,我怀疑是我没有使dsp生成外部访问,因此想咨询一下如何通过数据空间去访问外部存储器?感谢感谢