Part Number: AM5728
我想要通过串口接收数据,使用UART_read()接收数据,则必须实时调用UART_read()才能收到数据,故想到使用Hwi_create()接口创建硬件中断,但是如何关联到串口的接收中断呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
void hwiFunc(UArg arg)
{
unsigned char rxData = 0;
//在中断服务程序中清中断
//Hwi_clearInterrupt(7);
/* Checking ths source of UART interrupt. */
int32_t intId = UARTIntIdentityGet(SOC_UART1_BASE);
Log_print1(Diags_ENTRY, "UARTIsr: %d", intId);
switch (intId)
{
case UART_INTID_TX_THRES_REACH:
Log_print0(Diags_ENTRY, "UART_INTID_TX_THRES_REACH");
break;
case UART_INTID_RX_THRES_REACH:
rxData = UARTCharGetNonBlocking(SOC_UART1_BASE);
//UARTCharPutNonBlocking(uartBaseAddr, rxByte);
Log_print1(Diags_ENTRY, "Rx: %02x", rxData);
break;
case UART_INTID_RX_LINE_STAT_ERROR:
case UART_INTID_CHAR_TIMEOUT:
rxData = UARTCharGetNonBlocking(SOC_UART1_BASE);
if(intId == UART_INTID_CHAR_TIMEOUT)
Log_print1(Diags_ENTRY, "UART_INTID_CHAR_TIMEOUT: %02x", rxData);
else
Log_print1(Diags_ENTRY, "UART_INTID_RX_LINE_STAT_ERROR: %02x", rxData);
break;
default:
break;
}
}
void Hwi_Init(void)
{
Log_print0(Diags_ENTRY, "Hwi_Init");
//创建中断
Hwi_Handle hwi_uart1; //句柄
Hwi_Params hwi_params; //传入参数
Error_Block eb; //错误块
Error_init(&eb); //错误块初始化,注意必须初始化,否则易进入System_abort
Hwi_Params_init(&hwi_params); //初始化传入参数
hwi_params.eventId = 43;
hwi_params.enableInt = TRUE;
//hwi_params.maskSetting = Hwi_MaskingOption_SELF; // don't allow this interrupt to nest itself
hwi_uart1 = Hwi_create(7, hwiFunc, &hwi_params, &eb); //注意此处id是中断等级编号,如中断5,则id为5
if(hwi_uart1 == NULL)
{
System_abort("hwi_uart1 create failed");
}
Hwi_enableInterrupt(7); //使能中断
}我创建中断后,一直不能进入中断服务函数,串口这边的配置应该如何设置呢?是调用 PDK_INSTALL_PATH\packages\ti\csl\src\ip\uart\V1\uart.h 还是使用
PDK_INSTALL_PATH\packages\ti\drv\uart\UART.h 的库函数配置串口?