Part Number: TMS320C6678
目前编写了一个代码,通过核0对其他核发起局部复位,网络接收BIN并存放到指定的位置,再通过IPC信号唤醒其他核。
bin放在L2SRAM时可以正常运行,但是放在DDR3时产生异常第一次唤醒其他核后跑飞,第二次后又能正常。
memset(pBuf, 0, 13);
bytes = (int)recv(connfd, (void *)pBuf, 9, 0); //接收bin程序入口_c_int00地址
if(bytes != 8) {
uart_printf("File Head Error 1!bytes: %d!\n", bytes);
goto leave;
}
Entry_Address = strtohex(pBuf, 8);
memset(pBuf, 0, 13);
bytes = (int)recv(connfd, (void *)pBuf, 9, 0); //接收存放bin文件起始地址
if(bytes != 8) {
uart_printf("File Head Error 2!bytes: %d!\n", bytes);
goto leave;
}
WriteAddr = (unsigned int*)strtohex(pBuf, 8);
memset(pBuf, 0, 13);
bytes = (int)recv(connfd, (void *)pBuf, 2, 0); //ignore standard header
if(bytes != 1) {
uart_printf("File Head Error 3!bytes: %d! %s\n", bytes, pBuf);
goto leave;
}
corenum = pBuf[0] - 0x30; //接收需要替换代码的核号
uart_printf("%x %x %d\n", Entry_Address, (unsigned int)WriteAddr, corenum);
while (1) {
memset(pBuf, 0, 13);
bytes = recv(connfd, pBuf, 4, 0);
if (bytes <= 0) {
break;
}
*WriteAddr = littleToBig(pBuf);
WriteAddr++;
}
Load_Core_app_Start(Entry_Address, corenum);
....
....
....
void Load_Core_app_Start(unsigned int EntryAddr, int corenum)
{
unsigned int MAGIC_ADDR = 0X1087FFFC + corenum * 0x1000000;
CSL_BootCfgUnlockKicker();
CSL_PSC_setModuleLocalReset(corenum + 15, PSC_MDLRST_ASSERTED);
CSL_PSC_setModuleLocalReset(corenum + 15, PSC_MDLRST_DEASSERTED);
cpu_delaycycles(100000);
*((volatile unsigned int *)MAGIC_ADDR) = EntryAddr;
cpu_delaycycles(100000);
CSL_IPC_genGEMInterrupt (corenum, 0);
CSL_BootCfgLockKicker();
}