This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM6467T: 烧录程序经常失败,成功概率不足1%

Part Number: TMS320DM6467T

换了一块另一个厂家的DM6467T(不是以前俊竹科技的板子了),能烧录程序,但经常失败。失败原因罗列如下:

FTDI:
Error connecting to the target:
(Error -154 @ 0x0)
One of the FTDI driver functions used to
write data returned bad status or an error.
(Emulation package 9.6.0.00172)
HUNG:
Error connecting to the target:
(Error -1144 @ 0x0)
Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.6.0.00172)
PRSC:
Error connecting to the target:
(Error -6311) PRSC module failed to write to a register.
(Emulation package 9.6.0.00172)
RESET:
Error connecting to the target:
(Error -1137 @ 0x0)
Device is held in reset. Take the device out of reset, and retry the operation.
(Emulation package 9.6.0.00172)
DATA:
C64XP: File Loader: Verification failed: Values at address 0x8204D680 do not match Please verify target memory and memory map.
C64XP: GEL: File: /home/wzy/workspace_v11/x264/Debug/x264.out: a data verification error occurred, file load failed.

目前发现FTDI 的错误似乎重启CCS 可以解决,其他错误近乎无解。除此之外,发现一些规律:比如当电流为0.9A 时必定报错HUNG,当电流为0.55A 时必定报错RESET,PRSC除少数的0.7A 和 0.65A 外都为0.6A。 关于灯的亮度:如果灯亮(LIGHT)或闪烁(FLASH),无论闪烁后是继续亮还是熄灭必定电流为0.9A(除少数0.7A)。但电流为0.9A 不一定灯亮。未观察到灯的亮度和报错信息之间的关系。 当这块板子正常工作时,电流必定为0.9A,且指示灯明亮但不闪烁。可以通过亮度和闪烁预 先排除掉不可能正常工作的情况以节约重复时间。可以通过电流大小预先判断报错的原因。绝大多数错误以HUNG为主。有时HUNG 报错后电流会从0.9A 掉到0.6A,这时再次DEBUG报错会转为PRSC,还出现了2次 DATA。

每次尝试均插上仿真器,仿真器灯亮则上电,Debug,报错,断电,断开仿真器。

test connection 没有问题。

这块板子上没有RESET按钮。

感谢一切回复。