This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: load问题

Part Number: TMS320C6748

仿真器连接成功。程序编译也通过,但在load时报错,无法下载程序,报错如下:

C674X_0: Trouble Writing Memory Block at 0x8000 on Page 0 of Length 0x7040: (Error -1190 @ 0x8000) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.100.0)
C674X_0: File Loader: Verification failed: Target failed to write 0x00008000
C674X_0: GEL: File: E:\CCS7.4workspace\test\Debug\test.out: Load failed.

程序是最简单的helloworld