最近在小批量,焊了30块,有5块板启动时找不到内核,提示如下:启动方式10011 从MMC烧写到NAND 然后从nand启动的
NAND read: device 0 offset 0x700000, size 0x80000
524288 bytes read: OK
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0-ga894bde-dirty
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3089472 Bytes = 2.9 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
U-Boot#
使用mtest命令是这种:
U-Boot# mtest
Pattern 00000000 Writing... Reading...
Mem error @ 0x8434196C: found 000F065B, expected 000D065B
Mem error @ 0x846A0430: found 0018810C, expected 001A810C
Pattern FFFFFFFF Writing... Reading...
Mem error @ 0x8434196C: found FFF6F9A4, expected FFF2F9A4
Mem error @ 0x846A0430: found FFE77EF3, expected FFE57EF3
Pattern 00000001 Writing... Reading...
Mem error @ 0x8434196C: found 000F065C, expected 000D065C
Mem error @ 0x846A0430: found 0018810D, expected 001A810D
Mem error @ 0x846A0434: found 001A810C, expected 001A810E
Pattern FFFFFFFE Writing... Reading...
Mem error @ 0x8434196C: found FFF6F9A3, expected FFF2F9A3
怀疑是焊接或DDR质量问题,但是都重新焊接或者换了新的芯片,仍然是找不到内核!
请问各位有没有碰到过这种情况??