This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: 安装ti-processor-sdk-rtos-am57xx-evm-04.03.00.05-Linux-x86-Install最后,无法安装cgtxxx_installer

Part Number: AM5708


linux环境为ubuntu20.04

  • sdk和ccs都安装在默认路径下吗?看一下user gude Note部分Linux下的安装注意事项是否有忽略的部分。

    • When Installing on linux (Ubuntu 16.04 and above) the following packages need to be installed before the Procsdk RTOS installer is installed

      sudo apt install diffstat texinfo gawk chrpath dos2unix unzip socat doxygen libc6:i386 libncurses-dev:i386 libstdc++6:i386 libz1:i386

    • To avoid configuring CCS “Tool Discovery Path” to search for components in different directories, it is recommended to install the SDK in the same directory as CCS. This is C:/TI for Windows and /home/[user]/ti for Linux.

    software-dl.ti.com/.../index_overview.html