This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TIDL:是否有TIDLlayer支持CAFFE网络中的通道搬运或SCALE操作

Part Number: TDA4VM


问题:

(1)在SDK7.0.1中的TIDL,使用全连接层需要对输入做flatten操作。若网络输入一定,通道为N,C,H,W,在caffe中通过全连接层后size为1,64,1,1,在TIDL中则变为1,1,1,64。现有的TIDLlayer有没有手段实现1,1,1,64到 1,64,1,1的数据搬运。

(2)现有的TIDLlayer有没有CAFFE中SCALE层的操作,使得1,64,1,1中64个通道的数据对应相乘到另一个64通道的tensor上。

(3)如果没有上述功能,有什么手段可以在保证网络推断速度的前提下这些需求。