/**
* \brief EDMA3 Initialization
*
* This function initializes the EDMA3 Resource Manager for the given EDMA3 controller
* and opens a EDMA3 RM instance. It internally calls EDMA3_RM_create() and
* EDMA3_RM_open(), in that order.
*
* It also registers interrupt handlers for various EDMA3 interrupts like
* transfer completion or error interrupts.
*
* \param edma3Id [IN] EDMA3 Controller Instance Id (Hardware
* instance id, starting from 0)
* \param errorCode [IN/OUT] Error code while opening RM instance
* \return EDMA3_RM_Handle: If successfully opened, the API will return the
* associated RM's instance handle.
*/
EDMA3_RM_Handle edma3init (uint32_t edma3Id, EDMA3_RM_Result *errorCode);
typedef enum
{
CSL_XBAR_DMA_CPU_ID_SYSTEM_DMA,
CSL_XBAR_DMA_CPU_ID_EDMA,
CSL_XBAR_DMA_CPU_ID_DSP1_DMA,
CSL_XBAR_DMA_CPU_ID_DSP2_DMA
} CSL_XbarDmaCpuId;

我有多个外设需要用到EDMA,使用EDMA3 LLD库,遇到一些问题,希望TI工程师可以答疑。
问题1:edma3init() 函数的第一个参数 edma3Id,应该如何配置?是否按照 Table 16-125. EDMA_TPCC_PID 里的instance id配置,还是与 CSL_XbarDmaCpuId enum一致?
问题2:若多个外设都需要使用EDMA,每个外设都需要执行一次edma3init()吗?即EDMA3_RM_Handle是否是共用的?