This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5706: 使用2片DDR3L T拓扑结构可以省掉VTT端接电阻吗

Part Number: AM5706


使用2片DDR3L T拓扑结构可以省掉VTT端接电阻吗

  • 参考 2.11 DDR3

    Designs with point to point connections between the AM57xx devices and a single DDR3 SDRAM typically do not need VTT termination, although, this may be needed depending on the specific PCB characteristics. For multiple device topologies or multi-die packages, VTT termination is required. A VTT termination regulator is required for properly terminating the address, command and control fly-by signals

    www.ti.com.cn/.../sprack7b.pdf