This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: PSDK TIDL8.1:demo model pelee 浮点模式numParamBits=32 inference没有检测到目标

Part Number: TDA4VM

Hi, TIers,

基于TIDL demo model pelee && host emulation, 采用如下配置进行定点模式numParamBits=8的import and inference,能够得到正确的检测结果,但改为浮点模式 numParamBits=32 import and inference, 没有检测到目标,结果为全0. 配置如下(1)(2), 另外,浮点模式import有一个warning 如(3).

麻烦帮忙分析下原因,谢谢!

(1)  import config file 

modelType          = 0
numParamBits = 8
inputNetFile       = "../../test/testvecs/models/public/caffe/peele/pelee_voc/deploy.prototxt"
inputParamsFile    = "../../test/testvecs/models/public/caffe/peele/pelee_voc/pelee_304x304_acc7094.caffemodel"
outputNetFile      = "../../test/testvecs/config/tidl_models/caffe/tidl_net_peele_300.bin"
outputParamsFile   = "../../test/testvecs/config/tidl_models/caffe/tidl_io_peele_300_"
inDataNorm  = 1
inMean = 104 117 123
inScale = 0.0170000009239 0.0170000009239 0.0170000009239
inDataFormat = 0
inData  =   "../../test/testvecs/config/detection_list.txt"
postProcType = 2
perfSimConfig = ../../test/testvecs/config/import/device_config.cfg
inWidth  = 1024
inHeight = 512
inNumChannels = 3
foldMaxPoolInConv2D = 0
foldPreBnConv2D = 0

(2) inference config file

inFileFormat    = 2
postProcType = 2
#numFrames   = 272
numFrames   = 1
netBinFile      = "testvecs/config/tidl_models/caffe/tidl_net_peele_300.bin"
ioConfigFile    = "testvecs/config/tidl_models/caffe/tidl_io_peele_300_1.bin"
outData =   "testvecs/output/pelee.bin"
inData  =   "testvecs/config/detection_list.txt"
debugTraceLevel = 2
writeTraceLevel = 1
reservedCtrl = 2

(3) warning in float mode import

WARNING: [TIDL_E_DATAFLOW_INFO_NULL] ti_cnnperfsim.out fails to allocate memory in MSMC. Please look into perfsim log. This model can only be used on PC emulation, it will get fault on target.