你好:
另外我按照1.2. Building the SDK — Processor SDK Linux for AM335X Documentation 这个手册在ubuntu16.04上面编译的时候,又出现了下面这个错误,现在是16.04和18.04都不能编译,请问你们这个07版本要求的ubuntu版本又是多少?
NOTE: Executing Tasks
ERROR: input-utils-1.0-r0 do_compile: oe_runmake failed
ERROR: input-utils-1.0-r0 do_compile: Execution of '/media/wujl/yocto_ti/tisdk/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/input-utils/1.0-r0/temp/run.do_compile.1501' failed with exit code 1:
Make.config:1: *** empty variable name. Stop.
WARNING: /media/wujl/yocto_ti/tisdk/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/input-utils/1.0-r0/temp/run.do_compile.1501:1 exit 1 from 'exit 1'
ERROR: Logfile of failure stored in: /media/wujl/yocto_ti/tisdk/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/input-utils/1.0-r0/temp/log.do_compile.1501