This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
plan1,capture camera data and display to eDP in single openvx process,delay is 70 ~ 80ms
plan2,capture camera data in one openvx process and display to eDP in another openvx process,the delay is 60 ~ 160ms,the average is 120 ~ 130ms
I am sure the sw delay from camera capture to vxProcessGraph finish in plan1 and plan2 is almost .
The the average delay of plan2 is about 50~60ms more than plan1 . the margin of error of plan1 is about +- 5ms,but plan2 is about +-50ms.
What is the reason?
thanks.
Hi,
We've got your issue and escalated to E2E for more help, below is the link:
Please expect the response.
Thanks!
Hi,
Please address below queries.
1. By single process and multi process in Plan 1 and Plan2, do you mean that in plan 1, both capture and display is in the same graph? and in plan2 capture is in one graph and display is in another?
2. In Plan1, Does this graph only has capture node and display node?
In Plan2, again is it only capture node in one graph and only display node in another graph?
3. Where is the start and end point for calculating this delay? is it from output of capture node to first frame on display?
4. In Plan 2, are you dequeuing from one graph and enqueueing into the second?
Thanks.
1. Plan1, capture and display is in different graph . Plan2, caputre is in one graph in process1 and display is in one graph is prcess2
2. Yes, only caputre node and display node in plan1 and plan2. Plan1, capture and display is in different graph of 1 process, Plan2 , only capture node is in one graph in process1, only display node is in one graph iprocess2.
3. I use the GTC timestamp to calculate the code function time consuming ,and take a picture of ms timer and display to calculate the capture and display delay.
4. In Plan2, dequeue the capture data from caputre node and tivxReferenceExportHandle in prcocess 1 , get it by tivxReferenceImportHandle and display it in process2.
I find the delay of ipc of process1 and process2 is < 1ms, and the time consuming in vxProcessGraph is almost is Plan1 and Plan2 . So it is not enough to cause this problem.
Hi,
Understood the scenario in Plan 1.
Regarding the scenario in Plan 2, Could you please clarify if it is like a producer - customer scenario between two processes where the file descriptors are being exchanged?
Also Is it possible to share the source code in order to review it?
Thanks and regards,
Cherry
Yes, it is a server - client mode. The file descriptors is exchanged by binder.
In server process:
vx_reference ref;
tivx_utils_ref_ipc_msg_t ipcMsg;
ref = (vx_reference)pmap_info->image;
ret = tivx_utils_export_ref_for_ipc_xfer(ref, &ipcMsg);
if (ret != VX_SUCCESS)
{
LOGE("tivx_utils_export_ref_for_ipc_xfer() failed for object image");
break;
}
for(INT32 i=0; i<ipcMsg.numFd; i++)
{
fd32[i] = (int32_t)ipcMsg.fd[i];
if(fd_desp)
{
fd_desp[i] = fd32[i];
}
}
send fd_desp by binder .
In client process:
int32_t fd[VX_IPC_MAX_VX_PLANES];
int32_t numFd;
vx_reference ref ;
vx_image image;
reveive fd by binder
for(int32_t i =0; i<numFd; i++)
{
ipcMsg.fd[i] = fd[i];
}
ret = tivx_utils_import_ref_from_ipc_xfer(m_vxContext, &ipcMsg, &ref);
if(ret == VX_SUCCESS)
{
image = (vx_image)ref;
}
Hi,
In this scenario, as the IPC and vxProcessGraph doesn't seem to be the issue,
Could you measure the time when the thread is getting scheduled?
Also the time taken from Dequeue to enqueue.
Thanks.
HI,
I measuer the GTC time in differrnt process function. In the capture process, as the fps is 30, the interval time of dequeue is ablout 33.3ms, the measure interval time is same, the time taker form dequeue to enqueue is about 40 us ~ 80 us. I think it should be OK.
In the display process, I find the time of vxProcessGraph is from 1 ms to 21 ms in eDP out scenario , the cycle time is about 60 s( 1800 frames), but in n CSITx out scenario , the time of vxProcessGraph is always about 11 ms. It is the same in Plan1.
Is it a mormal condition?
what is the difference between one process and muti process in tiOpenVx framework ? for example :RAM ,DMA and other HW resource etc .
thanks
Hi,
The issue TIOVX-1132 was as mentioned below
This issue is fixed in SDK 8.1
May I know which SDK version are you using?
If the version is before SDK 8.1 could you try with below patch in the tiovx folder. This patch is the fix for the issue TIOVX-1132
/cfs-file/__key/communityserver-discussions-components-files/791/TIOVX_5F00_1132_5F00_Fix.zip