This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: SPI口主站/从站混用

Part Number: AM3352

AM3352有多个SPI口,是否可以主/从站混用,及SPI0(Pin A17,B17,B16,A16)用作从站,SPI1 (pin A13,D12,B13,C12)用作主站外接SPI FLASH。

如果可以,那寄存器MCSPI_MODULCTRL的bit2 MS 设置为0还是1?