现在使用场合是6678+4个DDR3,一个DDR3对应16位DQ数据,4个DDR3组成64bit的DQ数据,四个DDR3共用DSP的时钟,因为DDR3的数据信号采样是对应DQS(也对应DSP控制器的输出时钟CLK)的上升沿和下降沿,一个时钟周期采样两次数据,假如把6678与DDR3的接口配置成64bit位宽,6678与DDR3读/写数据的时候,在DSP输出时钟的一个上升沿周期内,DSP是不是就要在DDR3那边读/写64bit的数据,一个下降沿周期内,DSP也要从DDR3那边读/写64bit的数据,是这样吗?请论坛里面的大神指点一下,不胜感激。