Part Number: 66AK2H12
您好
在使用66AK2H12过程中,发现看门狗可以使用外部时钟并正常工作,这是芯片的bug?与手册描述有冲突?

望回复!
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问您是怎么确定watchdog timer用的是external clock? 如果把external clock去掉,watchdog timer不能工作了?
如果不配置TIMI1为输入时钟,watchdog能工作吗?看门狗应该没有外部时钟也能工作的。
另外,Timer16-19是不支持外部时钟的吧?
是的,TINPSEL寄存器只能配置timer15~0。请参考数据手册10.2.3.17 Timer Input Selection Register (TINPSEL)
https://www.ti.com/lit/ds/symlink/66ak2h12.pdf
您好谢谢回复
使用内部时钟是可以的。那我是不是可以认为,手册上面看门狗严格限制为外部时钟的描述是不准确的(起码对于66AK2H12这款芯片来说)呢?
另外最近在丰富Timer的底层驱动程序时,还有其他问题,请问可以在下面继续提问么?还是需要重新建一个新帖子?
问题1:关于外部时钟切换的问题,不理解英文描述的具体意思。如下图所示,请问如果定时器计数到10000后,需要切换为外部时钟并继续计数,需要怎么写驱动程序呢。我尝试了很多次,都不能成功。切换成外部时钟后就不能继续计数了。

问题2:手册中提到的定时器的复位bit(TIMLORS和TIMHIRS)描述好像也是不准确的。在我的驱动程序中发现,TIMLORS和TIMHIRS并不能清零(TSTAT_LO和TSTAT_HI)

谢谢,望回复!!