TI的专家您们好!目前我们使用EVM板已经可以进RGB1920x2160的分辨率,也可以进行编码,但我们需要验证3840x2160的分辨率,目前我想这样测试,先将1920x2160 通过dup成两个1920x2160, 然后将这两路通过 megre合并为3840x2160,然后进行编码,试了很久都不行,请问我这个方法可行吗?期待您们的回复!
另外,还想问一下8168的两个网口市独立的吗?有没有交换功能?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的专家您们好!目前我们使用EVM板已经可以进RGB1920x2160的分辨率,也可以进行编码,但我们需要验证3840x2160的分辨率,目前我想这样测试,先将1920x2160 通过dup成两个1920x2160, 然后将这两路通过 megre合并为3840x2160,然后进行编码,试了很久都不行,请问我这个方法可行吗?期待您们的回复!
另外,还想问一下8168的两个网口市独立的吗?有没有交换功能?
用merge的方法不可行
merge link是把多个input que合并成一个output que,而不是把两幅图像合并成一幅图像。
你的case里,merge的输出是1个que,但这1个que里有两路视频,仍然是独立的两路视频,即你dup出来的两路1920x2160视频。
Haijun Guo你好:
在Fvid2_pFrame()结构体中定义的addr这个是不是就是视频源的地址?
但是好几种格式怎么区分?在通过串口打印处理之后的是addr[0][0]是不断更新的,其他几个值都是0x6000 0000,想知道这个时候这个数据格式是什么样的?这个是首地址吗? 是不是通过地址偏移进行数据读取的?谢谢!!!