This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于EDMA的一个疑问



如果是手动触发的话,单核能否开启两个channel进行传输?我现在情况是按照例程定义了两个channel,分别映射不同的param,不同的TCC,但是当我第一次手动触发的时候,设置的传递参数是channe1,可是触发完成后发现,中断完成位确是对应的channel2的TCC。后来我发现无论我输入的是channel1 还是channel2,触发的都是channel2 param所对应的传输。。。

  • if (CSL_edma3Init(&context) != CSL_SOK)
    {
    printf ("Error: EDMA module initialization failed\n");
    }


    hModule = CSL_edma3Open(&edmaObj, INSTNUM, NULL, &status);
    if ( (hModule == NULL) || (status != CSL_SOK))
    {
    printf ("Error: EDMA module open failed\n");
    }


    chAttr.regionNum = CSL_EDMA3_REGION_GLOBAL; /*GLOBAL*/
    chAttr.chaNum= 0;
    hChannel1 = CSL_edma3ChannelOpen(&chObj, INSTNUM, &chAttr, &status);
    if ((hChannel1 == NULL) || (status != CSL_SOK))
    {
    printf ("Error: Unable to open EDMA Channel:%d\n", 0);
    }

    chAttr.chaNum= 1;
    hChannel2 = CSL_edma3ChannelOpen(&chObj, INSTNUM, &chAttr, &status);
    if ((hChannel2 == NULL) || (status != CSL_SOK))
    {
    printf ("Error: Unable to open EDMA Channel:%d\n", 1);
    }

    if (CSL_edma3HwChannelSetupQue(hChannel1,CSL_EDMA3_QUE_0) != CSL_SOK)
    {
    printf ("Error: EDMA channel setup queue failed\n");
    }

    if (CSL_edma3HwChannelSetupQue(hChannel2,CSL_EDMA3_QUE_0) != CSL_SOK)
    {
    printf ("Error: EDMA channel setup queue failed\n");
    }

    CSL_edma3MapDMAChannelToParamBlock (hModule, 0, 0);
    CSL_edma3MapDMAChannelToParamBlock (hModule, 1, 1);

    Param0= CSL_edma3GetParamHandle(hChannel1, 0, &status);
    if (Param0 == NULL)
    {
    printf ("Error: EDMA Get Parameter Entry failed for paramID.\n");

    }

    Param1= CSL_edma3GetParamHandle(hChannel2, 1, &status);
    if (Param1 == NULL)
    {
    printf ("Error: EDMA Get Parameter Entry failed for paramID.\n");

    }

    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
    CSL_EDMA3_TCCH_DIS, \
    CSL_EDMA3_ITCINT_DIS, \
    CSL_EDMA3_TCINT_EN, \
    0, CSL_EDMA3_TCC_NORMAL,\
    CSL_EDMA3_FIFOWIDTH_NONE, \
    CSL_EDMA3_STATIC_DIS, \
    CSL_EDMA3_SYNC_AB, \
    CSL_EDMA3_ADDRMODE_INCR, \
    CSL_EDMA3_ADDRMODE_INCR );


    myParamSetup.srcAddr = (Uint32)DDR;//源地址
    myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(4,512);//因为传输的是Uint32,所以每次array跳变是4byte,一共跳变512
    myParamSetup.dstAddr = (Uint32)mem;//目的地址,L2地址必须用全局地址
    myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(4,4);
    myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(0xFFFF,0);//无link
    myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);
    myParamSetup.cCnt = 1;

    if(CSL_edma3ParamSetup(Param0,&myParamSetup) != CSL_SOK)
    {
    printf ("Error: EDMA Parameter Entry Setup failed\n");
    }

    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
    CSL_EDMA3_TCCH_DIS, \
    CSL_EDMA3_ITCINT_DIS, \
    CSL_EDMA3_TCINT_EN, \
    1, CSL_EDMA3_TCC_NORMAL,\
    CSL_EDMA3_FIFOWIDTH_NONE, \
    CSL_EDMA3_STATIC_DIS, \
    CSL_EDMA3_SYNC_AB, \
    CSL_EDMA3_ADDRMODE_INCR, \
    CSL_EDMA3_ADDRMODE_INCR );

    myParamSetup.srcAddr = (Uint32)mem;//源地址
    myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(4,512);//因为传输的是Uint32,所以每次array跳变是4byte,一共跳变512
    myParamSetup.dstAddr = (Uint32)L2+ (0x10000000);//目的地址,L2地址必须用全局地址
    myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(4,4);
    myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(0xFFFF,0);//无link
    myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);
    myParamSetup.cCnt = 1;

    if(CSL_edma3ParamSetup(Param1,&myParamSetup) != CSL_SOK)
    {
    printf ("Error: EDMA Parameter Entry Setup failed\n");
    }

    regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
    regionIntr.intr = 0x0003; //中断使能位必须和所设置的TCC相同
    regionIntr.intrh = 0x0000;

    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,&regionIntr);

    regionIntr.intr = 0x0000;

    CSL_edma3HwChannelControl(hChannel1,CSL_EDMA3_CMD_CHANNEL_SET,NULL);

    do {
    CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,&regionIntr);
    } while (!(regionIntr.intr & 0x0001));//

    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,&regionIntr);

    CSL_edma3HwChannelControl(hChannel1,CSL_EDMA3_CMD_CHANNEL_SET,NULL);

    do {
    CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,&regionIntr);
    } while (!(regionIntr.intr & 0x0002));//

    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,&regionIntr);

  • 注意函数CSL_edma3ChannelOpen的内部实现,其返回值为hEdma = (CSL_Edma3ChannelHandle)pEdmaObj;所以按照你的这种配置顺序,每个channel在调用如下函数open channel时,其输入第一个参数必须不一样,否则返回值只会记录最后一个channel的参数,所以你的代码中在后面enable channel时使能的始终是channel2.

    CSL_Edma3ChannelHandle CSL_edma3ChannelOpen
    (
    CSL_Edma3ChannelObj* pEdmaObj,
    CSL_InstNum edmaNum,
    CSL_Edma3ChannelAttr* pChAttr,
    CSL_Status* pStatus
    )