This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【资料共享】SRIO编程及调测指南



附件是与之前发布的SRIO例程对应的编程指南手册,请参考。

SRIO_Programming_Performance.pdf
  • 请问一下,在帖子中你提到之前发布的SRIO例程,在哪里有下载,我正好需要SRIO例程,谢谢了

  • 软件开发包

    http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/47664.aspx

  • 谢谢了,太感谢了


  • Andy Yin1 你好。

        非常感谢提供这些例程,我是个新手,正在学习其中的SRIO例程,目前碰到一些问题:工程

    build成功后,无论是使用模拟器还是运行在EVM6678L开发板上,我都无法在C代码下F5单步跟踪程序;

        我copy例程中的SRIO和common两个文件夹到我的workspace文件夹中并导入SRIO工程到CCS5.4;

    修改了include路径与我的安装路径匹配,其中pdk我使用的是pdk_6678_1_1_2_5版本;
        
        build成功后用模拟器运行,会出现:
    Can't find a source file at "/tmp/TI_MKLIBy3wfGo/SRC/boot.c"
    Locate the file or edit the source lookup path to include its location.
        无法进入main();
        
        请教到底是哪里不对呢?

  • 你好,我用6678测试SRIO接口,速率3.125G,包的ftype=5,ttype=4,有时候会出现LSU_REG6_FULL现象,其他数据就发送不出去了,这个是什么引起的?怎么解决?

    还有如果我要配置成5G速率,除了要改SERDES_CFGPLL里的倍频数据外还有啥要改的?3.125G和5G参考时钟是一样的156.25,都是half rate。

    谢谢

  • 你好,我用6678测试SRIO接口,速率3.125G,包的ftype=5,ttype=4,有时候会出现LSU_REG6_FULL现象,其他数据就发送不出去了,这个是什么引起的?怎么解决? 还有如果我要配置成5G速率,除了要改SERDES_CFGPLL里的倍频数据外还有啥要改的?3.125G和5G参考时钟是一样的156.25,都是half rate。

  •       CONG WANG4:

                您好,我刚开始研究DSP,J接手C6678这块板子,我想问您一下为什么我的SRIO测试例程build不成功呢?我按照测试历程给的说明操作也是失败,您是如何build成功的呢?因为最近对这个比较急,望您看到后回复。