This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

新手求教:C66x多核编程



新手求教:C66x多核编程

1. 如何将任务定位到4个独立的core中运行?

2. 如何设置其中一个core为master,其他为slave model?

3. 多核编程一定需要用到SDK吗?

谢谢。

  • 答:

    1,core与core之间是独立的,除了内存(MSMC,DDR)和外设是共享之外。因此你可将一个大任务分为4个单独的小任务,然后每个核一个。

    2,这个是软件设置的,一般默认就是core0是master,主要是指在上电后core0最先运行,然后core0会boot其余core运行;

    3,SDK是个工具,方便用户在上面开发。如果有成熟的开发团队,一般可以自己开发多核。

  • 非常感谢楼上的回答!

    对于第三个问题,我想问一下:SDK 和 SYS/BIOS 什么关系?

    如果多核移植了SYS/BIOS系统,是否不需要用到SDK了?