AM335X 中那个可以驱动10寸屏,Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
每像素8bit分辨率高达2048x2048指的是LCD Controller最大能支持的frame buffer size。
126MHz扣除VSYNC/HSYNC(可编程,视屏幕模组的LCD控制器而定)就是最大的pixel输出能力,可以用来大致估算frame rate。
挑战高像素的时候实际的瓶颈是内存带宽,以及对android这种严重依赖于OpenGL的UI来说,GPU的性能。
335x,Android,如果CPU是1GHz,内存是DDR3-800(频率嗷嗷高但可惜是16bit,和手机比得打对折了),1024x600是肯定OK的,但基本上也是流畅的极限了。如果未来TI能把内存搞到DDR3-1333去,那么1280x720应该也可以搞定,如果能到DDR3-1600,1280x800也差不多了。
如果是Linux,1GHz/DDR3-800搞到1280x800问题不大。