This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tvp5158+ths8200四路输入合并成一路高清输出显示器不识别

Other Parts Discussed in Thread: TVP5158, THS8200

 我最近在尝试将tvp5158采集的四路信号拼接成一路的1080i50用ths8200输出,平台是dm6467+dvsdk_1_40_02_33,但是出现下面状况,不清楚是什么问题,

1)tvp5158四路信号采集没有问题,可以通过写文件的形式将拼接之后的图像输出;

2)ths8200的1080i50的输出也没有问题,可以直接读取文件输出,显示器可以显示;

3)但两个程序合并到一起后,采集的数据也没有问题,输出的视频波形是对的,但是里面的嵌入的一些同步信号不见了,显示器不能识别信号;比如720P60的正常视频输出示波器显示的是45.288kHz,但是将两者同时工作的输出频率是标准的45KHz,这一点很奇怪,后来检查发现少了一些输的那些波形,就是ths8200里面定义的FULL_NTSP和FULL_BTSP对应的波形,在这个时候如果撤去tvp5158的采集视频时钟,也就是5158不采集视频,ths8200就又可以输出了,显示器可以识别信号。

求论坛里大侠指导一二,多谢