This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM648 EDMA transfer controller register



求助,目前项目中使用的DSP芯片为DM648,项目中648会有较多的EDMA使用,在某些数据条件下会出现648死机,调试中发现EDMA transfer controller register中的某些寄存器值异常,

ERRSTAT0 = 0X0009,ERRDET0 = 0x13802;   

ERRSTAT1 = 0X0009,ERRDET1= 0x10009;

ERRSTAT2= 0X0009,ERRDET2 = 0x12901;

ERRSTAT3 = 0X0009,ERRDET3 = 0x13802;

而且在648没有死机,且数据正常的情况下,上面这些寄存器的值也是这样。关于这两个寄存器的说明可以在spec中查到,但是我认为不够详细,而且在648工作正常的状况下,这些寄存器的值也是上面写的,所以我的问题是这些值代表的意思,还有这两个寄存器有没有实际的参考价值