This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何查看DSP或者m3的输出信息求指导

Other Parts Discussed in Thread: TVP5158

不用仿真器,有办法么,我看到mcfw demo里面关于dsp和m3大量使用了一个Vps_printf函数打印一些东西实际运行时却是没有的,怎样才能看到这些信息呢,我想追踪下

  • http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/185162.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/228678.aspx

    大意就是你需要使能remote_debug_client.out

  • 你好关于终端输出信息询问下,是不是Vps_printf的输出信息前面肯定是有类似[m3vpss ]、[c6xdsp ]如果是a8输出的话就是没有的

  • 是的。类似于下图打印:

  • 感谢你的回答,但是还是有点疑惑:

    依次执行init.sh、load.sh和run.sh之后选择1模式:
    捕捉+编码+解码+显示。也就是:1: VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode

    我追踪McFw代码的时候,我记录了所有输出信息包括远程的m3和dsp,请看下面一段输出:
             [host] MCFW_IPCBITS:VcapVencVdecVdis_ipcBitsSendFxn:Entered...
             [host] MCFW_IPCBITS:VcapVencVdecVdis_ipcBitsRecvFxn:Entered...
             1: SYSTEM: System Common Init in progress !!!
             9: SYSTEM: IPC init in progress !!!
             21: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
             24: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
             26: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
             29: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
             30: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
             31: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
             33: SYSTEM: Notify register to [DSP] line 0, event 12 ...
             33: SYSTEM: Notify register to [VIDEO-M3] line 0, event 12 ...
             34: SYSTEM: Notify register to [VPSS-M3] line 0, event 12 ...
             35: SYSTEM: IPC init DONE !!!
             36: SYSTEM: Creating ListMP [HOST_IPC_OUT_29] in region 0 ...
             41: SYSTEM: Creating ListMP [HOST_IPC_IN_29] in region 0 ...
             44: SYSTEM: ListElem Shared Addr = 0x41671c80
             46: SYSTEM: Creating ListMP [HOST_IPC_OUT_30] in region 0 ...
             50: SYSTEM: Creating ListMP [HOST_IPC_IN_30] in region 0 ...
             53: SYSTEM: ListElem Shared Addr = 0x41689580
             55: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
             59: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
             63: SYSTEM: ListElem Shared Addr = 0x416a0e80
             65: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
             69: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
             72: SYSTEM: ListElem Shared Addr = 0x416c0480
             74: SYSTEM: Creating ListMP [HOST_IPC_OUT_26] in region 0 ...
             78: SYSTEM: Creating ListMP [HOST_IPC_IN_26] in region 0 ...
             82: SYSTEM: ListElem Shared Addr = 0x416dfa80
             82: SYSTEM: System Common Init Done !!!

            ********* Entered usecase 16CH Progressive <816x> Cap/Enc/Dec/Dis

             93: MCFW  : CPU Revision [ES1.1] !!!
             93: MCFW  : Detected [4x TVP5158 VS] Board !!!
             93: MCFW  : Base Board Revision [REV B] !!!
             93: MCFW  : Daughter Card Revision [REV B] !!!
             [m3vpss ]  1348225: HDMI: Starting HDMI Transmitter ... !!!
             [m3vpss ]  1348236: HDMI: HDMI Config ... DONE !!!
             .....
             .....
             [c6xdsp ]  1392086: IPC_FRAMES_IN   : Create in progress !!!
             [m3vpss ]  1354672: DUP   : Create Done !!!
             [c6xdsp ]  1392086: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_24] ...
             [m3vpss ]  1354672: IPC_FRAMES_OUT   : Create in progress !!!
             [c6xdsp ]  1392087: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_24] ...
             [c6xdsp ]  1392087: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
             [m3vpss ]  1354674: IPC_FRAMES_OUT   : Create Done !!!
             [c6xdsp ] IPC_FRAMES_IN:HEAPID:0       USED:240
             [c6xdsp ]  1392088: IPC_FRAMES_IN   : Create Done !!!
             [m3vpss ]  1354683: DEI    : Create in progress !!!
             [c6xdsp ] ALGLINK:HEAPID:0     USED:2832
             [c6xdsp ] ALGLINK:HEAPID:1     USED:5536
            从第3行开始到到33行都是A8的输出没错把,大部分是在一个System_init()函数及其子函数打印的。
            首先这个System_init()有4个定义,我知道分别是a8、dsp、m3vpss和m3video的分别实现,问题是:
            就我关注的dsp来说,下面这个打印出现在IpcFramesInLink_create()函数.
             [c6xdsp ]  1392086: IPC_FRAMES_IN   : Create in progress !!!
             调用关系如下:
            IpcFramesInLink_create()<--IpcFramesInLink_tskMain()<-IpcFramesInLink_init()<-System_init()
            请注意这里的 System_init函数有4个定义但是针对dsp的情况我选择对应dsp的System_init
            在dsp的System_init函数有这样的打印:
    #ifdef SYSTEM_DEBUG /*这个是有定义的*/
                Vps_printf(" %d: SYSTEM  : System DSP Init in progress !!!\n",
                           Clock_getTicks());
    #endif
            但是实际上串口是没有打印这一句的,后面还有很多句没有打印。
            这是为什么?
            我认为m3vpss和m3video的System_init都有执行到,但是部分信息都没有打印出来这是为什么?



            竟然在运行load.sh中发现上面本应该有的输出,能解释下么

  • 你确定你的SYSTEM_DEBUG这个宏定义了吗?

  • 你好我怀疑是先通过load.sh运行了两个m3和dsp也就是执行了System_init函数,然后一直等待a8的消息