This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运行DVSDK 2.0中的demo编译错误



我用的是DM6467的开发板,将原DVSDK1.4升级到2.0后,编译报错,是否我的工具安装有错。

root@davinci-desktop:/home/davinci/dvsdk_2_00_00_22/dvsdk_demos_2_00_00_07/dm6467/encode# make

======== Building encode ========
Configuring application using encode.cfg

making package.mak (because of package.bld) ...
generating interfaces for package encode_config (because package/package.xdc.inc is older than package.xdc) ...
configuring encode.x470MV from package/cfg/encode_x470MV.cfg ...
Info: Configuring engine named 'encode' from the info file for DSP server './encodeCombo.x64P',
          located in package 'ti.sdo.servers.encode':
      Target app will look for the DSP server image 'encodeCombo.x64P' in its current directory.
      Adding codec 'h264enc' (ti.sdo.codecs.h264enc.ce.H264ENC), scratch groupId=0
      Adding codec 'aacheenc' (ti.sdo.codecs.aacheenc.ce.AACHEENC), scratch groupId=1
      Adding codec 'g711enc' (ti.sdo.codecs.g711enc.ce.G711ENC), scratch groupId=1
Info: Reading DSP memory map from the info file for DSP server './encodeCombo.x64P',
      located in package 'ti.sdo.servers.encode':
js: "/home/davinci/dvsdk_2_00_00_22/xdctools_3_10_03/packages/xdc/xdc.tci", line 296: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: /home/davinci/dvsdk_2_00_00_22/dmai_1_20_00_06/packages/ti/sdo/dmai/package.xdc found along the package path, but no schema file was found.  Ensure that the package 'ti.sdo.dmai' is completely built.
    "/home/davinci/dvsdk_2_00_00_22/dvsdk_demos_2_00_00_07/dm6467/encode/encode.cfg", line 33
    "./package/cfg/encode_x470MV.cfg", line 479
    "./package/cfg/encode_x470MV.cfg", line 434
gmake: *** [package/cfg/encode_x470MV.c] 错误 1
js: "/home/davinci/dvsdk_2_00_00_22/xdctools_3_10_03/packages/xdc/tools/Cmdr.xs"