This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748开发UART程序



各位开发者:

           大家好。我运行Dbiospsp_03_00_01_00\drivers\examples\evm6748下的uart例程,发现main函数中有个configureUart()函数,找不到它的定义和实现在什么地方?麻烦知道的朋友告诉下,谢谢。

  • 在biospsp_03_00_01_00\platforms\evm6748\src的uart_evmInit.c中。

  • Hank Zhao,你好。我在CCS 5上跑biospsp_03_00_01_00\drivers\examples\evm6748下的uart例程,添加了各种库文件后,连上的开发板为TMDLCDK6748,导入生成的.out文件后,然后执行Resume操作,结构发现程序很久都执行没有终止,这个uart例程还需要硬件上的连接吗?

    例程的主函数如下:

    Void main(Void)
    {
    System_printf("\r\nUart Sample Main\n");

    /* Call the EVM specific initialization function */
    configureUart();

    BIOS_start();

    return;
    }

    我加断点进行调试,发现执行BIOS_start()时,程序就卡住了。不清楚什么原因。