This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678EVM板如何点亮LED灯?



板上有4个FPGA的debug灯,指南上说6678可以通过修改FPGA的配置寄存器SPI base+08h地址的寄存器值,点亮或熄灭led灯

问题:此处SPI base+08h如何理解,SPI是串行的,应该没有基址的概念。我的理解是通过6678 SPI口的片选CS1,把FPGA当成一个SPI存储器,往里面写数据,那么写进去的第9个数据就算是修改SPI base+08h寄存器的值了吗?

如果上面理解正确的话,我如何修改SPI读写SPI nor flash的程序,实现这种功能,FPGA没有页大小的概念初始化函数如何修改,读写函数的用法还一样吗?

写前还需要擦除操作吗?对FPGA应该不需要擦除

谁有6678控制FPGA 的SPI base寄存器的程序吗?