看到 TMS320C6416 DSK Technical Reference 里面,看到管脚 EMU0到EUMU11连接到一个HEADER,只有EMU0到EMU1又从该HEADER又被引回,接到jtag上,而并未看到该HEADER 连接到另外一个端口,即:EMU2到EMU11应该是被悬空了?是我看图有问题,还是这个电路就是这样的?或能否明确告知EMU2到EMU11应该如何连接,另外右边那些接地有何种用途,感觉右边那些接地仅仅是连接到此HEADER,而没有再从header处引出,有何功能?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看到 TMS320C6416 DSK Technical Reference 里面,看到管脚 EMU0到EUMU11连接到一个HEADER,只有EMU0到EMU1又从该HEADER又被引回,接到jtag上,而并未看到该HEADER 连接到另外一个端口,即:EMU2到EMU11应该是被悬空了?是我看图有问题,还是这个电路就是这样的?或能否明确告知EMU2到EMU11应该如何连接,另外右边那些接地有何种用途,感觉右边那些接地仅仅是连接到此HEADER,而没有再从header处引出,有何功能?
你好,
EMU2~EMU11是保留管脚, 悬空不接, 具体可以参考数据手册第42页上管脚说明.
http://www.ti.com/lit/ds/symlink/tms320c6416.pdf
这个是预留的60pin JTAG header, EVM板上只用14pin JTAG header