This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320VC5509A HPI 加载方式问题请教!



DSP型号为5509A,板子是我们自己做的,现在是脱机阶段!想把已经调试好的程序通过HPI方式加载,按照TI文档提供的顺序将生成的bin文件加载到DSP后,并不能正常工作,我们的设置如下:

1.批处理文件设置:hex55.exe -bootorg -v5510:2 -memwidth 8 -romwidth 16 -map LED.mxp LED.out -e 0x1400 -b -o LED.bin (其中-e 0x1400是根据map文件中

ENTRY POINT SYMBOL: "_c_int00"  address: 0x1400

2.CCS中build options->linker中的设置为:-q -c -e0x1400 -m".\Debug\LED.map" -o".\Debug\LED.out" -x  

3,cmd文件:

-w
-stack 0x1200
-sysstack 0x400
-heap  0x600
-lrts55x.lib
MEMORY                  
{
 PAGE 0:
     VECS    : origin = 0000100h, length = 0000100h
  /*HPIRAM:  origin = 0200h    length = 0700h*/


  DARAM:  origin = 0200h    length = 06000h
  /*DARAM1: origin = 06200h    length =1200h*/
     ROM:  origin = 0010000h    length = 02FFF0h

}

SECTIONS                
{
    .vectors  : {} > VECS  PAGE 0
    .text:    >   DARAM PAGE 0
    .data:    >   DARAM PAGE 0
    .cinit    >   DARAM PAGE 0
    .bss:     >   DARAM PAGE 0
 .cio:     >   DARAM PAGE 0
    .const    >   DARAM PAGE 0
    .stack    >   DARAM PAGE 0
    .sysstack >   DARAM PAGE 0
 .csldata:     >   DARAM PAGE 0
    .dmaMem:   {} > DARAM PAGE 0
 .voicedata:   {} > DARAM PAGE 0
 .sysmem:   {} > DARAM PAGE 0
 .sourdata :   {} > DARAM   PAGE 0
 .hpiRam:   {} > DARAM PAGE 0
 .hpiRam1:   {} > DARAM PAGE 0
}

 经过上面的设置后,将生成的bin文件通过HPI 加载到DSP后(经过对比加载的数据是正确的),并不能正常工作,load symbols only 单步运行后发现根本进不了main函数,将build options中的选项-c-改成cr后可以进main函数,但是在main函数运行的时候很多csl库中的函数根本没起作用,程序也不能正常工作,我想问下正确的HPI加载方式还需要设置什么地方?