This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我正在设计DM368的硬件电路,TI有一篇文档slvu730,推荐使用TPS650061来为DM368供电,其中,1.8V的最大输出电流为300mA,改文档同时指出,DM368的1.8V最大电流为125mA。
我看到EVM DM368的电路中,DM368的1.8V供电和DDR是采用同一个电源轨道,但DDR芯片MT47H64M16HR-25E的手册中,操作DDR时最大电流将达到 440mA。
这样,DM368和DDR共用的1.8V电源轨道将远远超过300mA。
请问:
1.DM368和DDR共用1.8V电源轨道是不是要保证同时上电?
2.是不是一定要用同一个电源轨道?
3.DM368和DDR在实际使用的时候电流有没有这么大?
4.在使用TPS650061为DM368供电的情况下,DDR的供电应该如何处理?
谢谢