This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于AM3359 最新am335x-evm-sdk-src-05.07.00.00.tar.gz的问题



下载了最新的开发包:am335x-evm-sdk-src-05.07.00.00.tar.gz 调试u-boot时使用以下命令

# make ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- am335x_evm_config

# make ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi-

问题1:绿色是自己的打印信息,而红色的musb,怎会在这里就启动?这个新的sdk包跟以往的差别大吗!

问题2TICCS5能否调试u-boot

U-Boot SPL 2013.01.01 (May 30 2013 - 20:45:54)
config_ddr(266)
s_init end
am33xx_spl_board_init
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img


U-Boot 2013.01.01 (May 30 2013 - 20:45:54)

I2C: ready
DRAM: 512 MiB
WARNING: Caches not enabled
board_init
board_init end
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment

musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
** Unable to read file uEnv.txt **
reading uImage
2922224 bytes read in 348 ms (8 MiB/s)
Booting from mmc ...
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Arago/3.1.0-psp04.06.00.03.sdk/a
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2922160 Bytes = 2.8 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.1.0 (jenkins@sdit-build01) (gcc version 4.5.3 201
10311 (prerelease) (GCC) ) #1 Sun Dec 11 12:45:19 CST 2011
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pag
es: 130048
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 r
o rootfstype=ext3 rootwait ip=none
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 513620k/513620k available, 10668k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffa00000 - 0xffe00000 ( 4 MB)
[ 0.000000] vmalloc : 0xe0800000 - 0xf8000000 ( 376 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0534000 (5296 kB)
[ 0.000000] .init : 0xc0534000 - 0xc056d000 ( 228 kB)
[ 0.000000] .data : 0xc056e000 - 0xc05c2d80 ( 340 kB)
[ 0.000000] .bss : 0xc05c2da4 - 0xc05fd320 ( 234 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrup
ts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER1 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER2 at 24000000 Hz
[ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 17895
6ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000234] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320)
[ 0.048808] pid_max: default: 32768 minimum: 301
[ 0.048958] Security Framework initialized
[ 0.049077] Mount-cache hash table entries: 512
[ 0.049509] CPU: Testing write buffer coherency: ok
[ 0.054760] print_constraints: dummy:
[ 0.055189] NET: Registered protocol family 16
[ 0.055576] GPMC revision 6.0
[ 0.058018] OMAP GPIO hardware version 0.1
[ 0.060717] omap_l3_smx omap_l3_smx.0: couldn't find resource
[ 0.061326] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.064999] omap_i2c.1: alias fck already exists
[ 0.066828] omap2_mcspi.1: alias fck already exists
[ 0.067110] omap2_mcspi.2: alias fck already exists
[ 0.094978] bio: create slab <bio-0> at 0
[ 0.097028] SCSI subsystem initialized
[ 0.099709] usbcore: registered new interface driver usbfs
[ 0.100119] usbcore: registered new interface driver hub
[ 0.100374] usbcore: registered new device driver usb
[ 0.118892] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
[ 0.121291] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.122539] Switching to clocksource gp timer
[ 0.128825] Switched to NOHz mode on CPU #0
[ 0.141384] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.141596] musb-hdrc musb-hdrc.0: dma type: pio
[ 0.142674] musb-hdrc musb-hdrc.0: USB OTG mode controller at e080a000 using
PIO, IRQ 18
[ 0.143470] musb-hdrc musb-hdrc.1: dma type: pio
[ 0.144446] musb-hdrc musb-hdrc.1: USB OTG mode controller at e080c800 using
PIO, IRQ 19
[ 0.144920] NET: Registered protocol family 2
[ 0.145148] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.145513] TCP established hash table entries: 16384 (order: 5, 131072 bytes
)
[ 0.145904] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.146131] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.146147] TCP reno registered
[ 0.146163] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.146193] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.146427] NET: Registered protocol family 1
[ 0.146760] RPC: Registered named UNIX socket transport module.
[ 0.146778] RPC: Registered udp transport module.
[ 0.146790] RPC: Registered tcp transport module.
[ 0.146801] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.147059] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.169862] VFS: Disk quotas dquot_6.5.2
[ 0.169944] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.170614] JFFS2 version 2.2. (NAND) (SUMMARY) 漏 2001-2006 Red Hat, Inc.
[ 0.170975] msgmni has been set to 1003
[ 0.171883] io scheduler noop registered
[ 0.171901] io scheduler deadline registered
[ 0.172001] io scheduler cfq registered (default)
[ 0.173241] Could not set LED4 to fully on
[ 0.175126] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.177114] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.658571] console [ttyO0] enabled
[ 0.662938] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.670781] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.678651] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.686482] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.694310] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.713104] brd: module loaded
[ 0.722144] loop: module loaded
[ 0.725960] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.732445] i2c-core: driver [tsl2550] using legacy resume method
[ 0.738948] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.802588] No daughter card found
[ 0.806206] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.872589] AM335X: EVM Config read fail: -110
[ 0.879183] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 0.886294] omap2-nand driver initializing
[ 0.890863] OneNAND driver initializing
[ 0.896701] CAN device driver interface
[ 0.900747] CAN bus driver for Bosch D_CAN controller 1.0
[ 0.907385] usbcore: registered new interface driver cdc_ether
[ 0.913803] usbcore: registered new interface driver cdc_subset
[ 0.920089] Initializing USB Mass Storage driver...
[ 0.925487] usbcore: registered new interface driver usb-storage
[ 0.931816] USB Mass Storage support registered.
[ 0.936763] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.942435] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe
r 1
[ 0.950384] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.957558] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=
1
[ 0.965180] usb usb1: Product: MUSB HDRC host driver
[ 0.970408] usb usb1: Manufacturer: Linux 3.1.0 musb-hcd
[ 0.976015] usb usb1: SerialNumber: musb-hdrc.1
[ 0.981713] hub 1-0:1.0: USB hub found
[ 0.985729] hub 1-0:1.0: 1 port detected
[ 0.991090] mousedev: PS/2 mouse device common for all mice
[ 0.998333] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[ 1.005121] omap_rtc: already running
[ 1.009232] i2c /dev entries driver
[ 1.015692] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.022689] cpuidle: using governor ladder
[ 1.027604] cpuidle: using governor menu
[ 1.035138] usbcore: registered new interface driver usbhid
[ 1.041013] usbhid: USB HID core driver
[ 1.041013] usbhid: USB HID core driver
[ 1.054582] ALSA device list:
[ 1.057711] No soundcards found.
[ 1.061289] oprofile: hardware counters not available
[ 1.066650] oprofile: using timer interrupt.
[ 1.071176] nf_conntrack version 0.5.0 (8025 buckets, 32100 max)
[ 1.078160] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.083930] TCP cubic registered
[ 1.087337] NET: Registered protocol family 17
[ 1.092029] can: controller area network core (rev 20090105 abi 8)
[ 1.098673] NET: Registered protocol family 29
[ 1.103374] can: raw protocol (rev 20090105)
[ 1.107873] can: broadcast manager protocol (rev 20090105 t)
[ 1.113892] Registering the dns_resolver key type
[ 1.118947] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
rev 3
[ 1.127053] ThumbEE CPU extension supported.
[ 1.132402] _regulator_get: mpu.0 supply mpu not found, using dummy regulator
[ 1.140069] omap2_set_init_voltage: Fail set voltage-mpu(f=600000000 v=120000
0)on vddmpu
[ 1.148615] omap2_set_init_voltage: unable to set vdd_mpu
[ 1.156932] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:11 UT
C (946684811)
[ 1.166306] Waiting for root device /dev/mmcblk0p2...