This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM6467 B17脚24M晶振不工作的问题,跪求



做了5块板,24M晶振均不工作,B15脚连接的27M晶振是正常工作的,急有思路来解决。

已做如下检查:

1.上电后27M两端对地电压为0.9V,24M两端对地电压为0.2V左右

2.把24M和27M晶振均去掉,上电,27M晶振晶振焊盘对地0.9V,24M晶振对地0.2-0.3V

3.2对PLLVDD电压正常

4.6467上电顺序正常

5.复位正常

6.晶振和18pf电容焊接良好,无虚焊

7.晶振质量没问题,用在其它板是可以工作的

最后一个办法就是回炉6467了,但是不可能5块板子6467的焊接都有问题吧?望求大侠给点思路,谢谢