AM335x目前支持哪些厂家的eMMC启动啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!可以参考AM335X TRM的说明:
Each interface has booting restrictions on which type of memory it supports: -
• MMC0 supports booting from the MMC/SD card cage and also supports booting from
eMMC/eSD/managed NAND memory devices with less than 4GB capacity.
• MMC1 supports booting from eMMC/eSD/managed NAND memory device with 4GB capacity or
greater.
The restriction is a result of many eMMC devices not being compliant with the eMMC v4.41 specification.
If you have the need to boot from two different card cages, many MMC/SD cards will boot from MMC1, but
for maximum compatibility only MMC0 should be used to boot from the card cage. Similarly for maximum
compatibility, booting from eMMC/eSD/managed NAND should only be performed on MMC1.
ben xue 说:你好,秦工,有没有可能用4G的eMMC作为启动芯片,会不会有问题?
请查看trm中的下述说明:
26.1.7.5.2 System Interconnection
Each interface has booting restrictions on which type of memory it supports: -
• MMC0 supports booting from the MMC/SD card cage and also supports booting from
eMMC/eSD/managed NAND memory devices with less than 4GB capacity.
• MMC1 supports booting from eMMC/eSD/managed NAND memory device with 4GB capacity or
greater.
看您用的是哪个mmc口做启动了