This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678,OpenMP,GCC

你好,

我现在用的OpenMP的支持包的版本是omp_1_01_02_06,我知道CCS5.2将GCC作为OpenMP的编译器,它是兼容OpenMP标准协议3.0版和GCC 4.5版的,但是不知道它是否支持GOMP_CPU_AFFINITY环境变量,因为它是GCC自带的?

还有就是如果支持OpenMP这些环境变量,那它们可以在哪里进行修改?是在我的电脑->属性->。。。里面,还是可以直接在CCS5里面修改,可以的话,具体在哪个位置?

谢谢!

  • 你好  请问你的问题解决了吗 ?  我现在也遇到类似的问题,请问一下 怎么样才能在CCS5中应用OpenMP进行编程呢?我的CCS5中没有OMP.h的头文件,请问我该怎么办?谢谢!