This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8168: 多路D1编码保存后视频文件卡顿

Part Number: TMS320DM8168
Other Parts Discussed in Thread: TVP5158

在使用DM8168 + 4片TVP5158,实现16路D1 采集、编码、保存h264的功能,使用的rdk版本: DVRRDK-04.01.00.02。

16路的link链路: cap --> Nsf -->  Dei1 + Dei2 --> MergeLink --> Encode --> Host

功能已经实现,但是在查阅保存的h264文件中发现,所有保存的h264文件播放有明显的卡顿。

尝试将16个编码通道 的scaleMode 更改为 352*288画面后实验,但保存的h264文件播放有明显的卡顿,效果没有改善。

重新构建新的测试程序,构建8路采集、编码、保存后的文件都是正常的,没有任何卡顿

8路的link链路: cap --> Nsf -->  Dei1 --> MergeLink --> Encode --> Host

请问是否有相关的配置能够优化此功能,或者还可能存在哪些问题点会导致此种情况?

 

  • 你好,

    默认的DVR RDK就有一个use case是Enc: 16Ch D1 30fps + 16Ch CIF 30fps + 16CH JPEG 1fps, Dec: 16Ch D1 30fps,你是参考的这个use case 代码么?

    请问你的硬件是TI的EVM还是自己的硬件,如果是自己的硬件,DDR SW leveling是否有做过,并把相应参数更新到uboot里?