This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4379: QSPI的时钟速度

Part Number: AM4379

从AM4379的资料中看到QSPI支持48M的时钟速度。“AM437x Sitara 处理器 数据表 (Rev. D)”的表5-95. 

另外,spruhl7i的表5-8中,在ROM代码中QSPI_CLK为12M。

测试发现只有12M,使用的是自编代码。测量位置为AM4379的B12,即QSPI_CLK,与外部FLASH连接的引脚。

在CCS中查看寄存器,QSPI_CLOCK_CNTRL_REG 的  DCLK_DIV是0, CLKEN 是1

如何配置才能使时钟速度为48M?或者说连接到外部FLASH时,QSPI_CLK并不能达到48M?

谢谢!