This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4 YUV422 sensor接在了tda4的csi1上,请问怎么配置csi这块

Part Number: TDA4VM


hi  ti专家:

   目前我司调试的yuv422 sensor接在了tda4的csi1上,请问一下如何配置在csi1上?

   现在测量解串器输出信号mipi clk, data信号均正常,

    我们使用的sdk版本是ti-processor-sdk-rtos-j721e-evm-08_01_00_11,使用的测试程序是vision_apps\apps\basic_demos\app_single_cam

   sensor配置如下:

   {
SENSOR_MAX9295A_DS, /*sensor name*/
0x1, /*i2cInstId*/
{
SENSOR_0_I2C_ALIAS, SENSOR_1_I2C_ALIAS, SENSOR_2_I2C_ALIAS, SENSOR_3_I2C_ALIAS,
SENSOR_4_I2C_ALIAS, SENSOR_5_I2C_ALIAS, SENSOR_6_I2C_ALIAS, SENSOR_7_I2C_ALIAS
},/*i2cAddrSensor*/
{
SER_0_I2C_ALIAS, SER_1_I2C_ALIAS, SER_2_I2C_ALIAS, SER_3_I2C_ALIAS,
SER_4_I2C_ALIAS, SER_5_I2C_ALIAS, SER_6_I2C_ALIAS, SER_7_I2C_ALIAS
},/*i2cAddrSer*/
/*IssSensor_Info*/
{
{
MAX96712_OUT_WIDTH, /*width*/
MAX96712_OUT_HEIGHT, /*height*/
1, /*num_exposures*/
vx_false_e, /*line_interleaved*/
{
// #ifdef ZYP_RAW_SENSOR
// {TIVX_RAW_IMAGE_P12_BIT, 11},
// #else
{VX_DF_IMAGE_UYVY, 7}, /*dataFormat and MSB [0]*/
//#endif
},
0, /*meta_height_before*/
0, /*meta_height_after*/
},
ISS_SENSOR_MAX96712_FEATURES, /*features*/
ALGORITHMS_ISS_AEWB_MODE_NONE, /*aewbMode*/
30, /*fps*/
4, /*numDataLanes*/
{1, 2, 3, 4}, /*dataLanesMap*/
{0, 0, 0, 0}, /*dataLanesPolarity*/
CSIRX_LANE_BAND_SPEED_1750_TO_2000_MBPS, /*csi_laneBandSpeed*/
},
8, /*numChan*/
390, /*dccId*/
}

麻烦帮忙看看,谢谢!