我实验了下CCS3.3的example,C:\CCStudio_v3.3\examples\dsk5416\csl\dma\dma4,发现测试打印的log一直停留在<DMA4>的位置,CCS3.3出现光标停在空白行,我想这个例子应该是可以没有问题,请教下是什么原因导致的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我实验了下CCS3.3的example,C:\CCStudio_v3.3\examples\dsk5416\csl\dma\dma4,发现测试打印的log一直停留在<DMA4>的位置,CCS3.3出现光标停在空白行,我想这个例子应该是可以没有问题,请教下是什么原因导致的?
你试试dma1, timer和mcbsp1自环例程, 看是否能运行? 如果只是mcbsp1不能运行, 其他两个可以运行的话, 可能mcbsp模块有问题了.
旧板子, 我上网查了下其他参考例子,增加了 PMST=PMST&0XFF, 发现在板子上可以正常运行,进中断。但是如果在SIMULATOR环境下,加这一句,则会出现反复进入main()函数的情况,类似打印如下:
<TIMER>
TEST PASSED
<TIMER>
TEST PASSED
不是很理解为什么这句话可解决这个问题,但是又会导致在SIMULATOR上发生这样的异常情况。补充:在板上,运行的gel文件,对PMST初始化=0XFFE0, 在SIMULATOR环境下初始化=0XFFE8.