This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: SD卡无法启动

Part Number: AM5718


板卡采用eMMC1的SD卡无法启动,使用示波器测量eMMC的CLK从400kHz变为12MHz左右,但无法启动,查看使用手册,该启动模式最低时钟可以为10MHz。测量开发板的该时钟信号可以达到48MHz,不知道是否与此速度有关。

另外使用AM571X的测试程序测试SD卡读写,不管开发板还是自制板卡的读写速度都是10MB左右,请问还有什么地方可以检查吗?或者U-BOOT是否可以配置启动速度,又怎么配置UBOOT