This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748通过SPI接口控制AD进行采样



各位开发者:

     大家好。我现在需要通过C6748的SPI接口来控制AD7466进行数据采样。采样频率为5k,数据为12位,每次总共采120秒,然后对采样数据进行处理。之前没做过相关的东西,现在有几个问题请教:

    1. 如何在程序中让SPI接口的SPI_CLK输出一个5k的采样脉冲?

    2. 每次采样600000个数据,我把它存在SDRAM中,SDRAM的大小为2G,我可以在程序中直接定义一个长度为600000的数组来存储采样数据吗?如果不可以的话,该如何来存储这些数据?

  • 你好,

    1. SPI clock是由SYSCLK2分频得来的, 而SYSCLK2由是由PLLDIV2寄存器对CPU clock分频得来的, 所以配置PLLDIV2和SPIFMT寄存器分频系数得到你要的5k时钟.
    SPIx_CLK frequency = [SPI module clock] / [SPIFMTn.PRESCALE + 1]

    你要看一下PLL章节和SPI章节的clock部分.

    2. 可以, 只要有足够的空间, 数组大小没有限制.