This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 PCIe 时钟丢失



各位高手:

   我自己做的6678的板子,6678是PG1.0的,PCIe的接口是符合普通计算机机箱的,但是一插上自己做的板卡,计算机就会把时钟关了,这是怎么回事呢?

  • 您好,

    请问你的板子上电及时钟等测试通过没,可以通过仿真器链接上么?如果都是可以的话,请把板卡配置成PCIe boot后,通过仿真器连上,查看相关PCIe 配置寄存器是否正常,如查看BAR寄存器的配置是否符合硬件设计的要求。

  • 板子上电这些没问题,DDR3都测了的,通过仿真器是可以连上的啊。为什么要把板卡配置成PCIe boot?我现在用的代码就是6678自带的PCIE_exampleProject。到LOCK那一步就进入死循环了,示波器一看,主机都把板卡的时钟屏蔽了,这个时候还没到BAR配置这些啊?可能我理解有误,多多指导啊!谢谢